AXIS#.IL.FRICTION

Description

Position command derivative sign is multiplied by this value to be injected to the current command.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

0 to the minimum of user positive current limit (AXIS#.IL.LIMITP) and motor peak current (AXIS#.MOTOR.IPEAK).AXIS#.IL.LIMITP

Default Value

0

Data Type

Float

See Also

AXIS#.IL.FF

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.FRICTION 0x500A 0xB DINT 1000:1 - RW False
AXIS2.IL.FRICTION 0x510A 0xB DINT 1000:1 - RW False